This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5066I: Follow-up: LM5066I telemetry behaviour

Part Number: LM5066I


Tool/software:

Hi,

this is a follow-up of the previous post I made about some strange LM5066i telemetry behaviour.

It has been quite a while since then, but in the meantime I have received the LM5066i EVK. To be comparable to our own design, I replaced the sense resistor with a 47mR resistor and increased Rpwr and Ctimer.

When I use that setup, I see basically the same behaviour as with our own design. When I increase the current in constant steps, I see ranges where the Iin raw ADC value does not change for 2 or three mV of voltage across Rsense.

In the low load range, the Iin value measured has a very big variance. So for example in this picture I have a current of 150mA, which corresponds to a voltage across the sense resistor of about 7mV. CL is set to 26mV, so 7mV means we're at about a quarter of the range here, and what I see is something like this:

So here I'm far off +/- 10% accuracy, which would be acceptable.

The variance gets less when I use bigger currents. This is for 300mA, corresponding to 14mV across Rsense:

So here we're around +/- 10% of the expected value, that would be OK, but also not really great.

So the question is: Is it expected that the accuracy of the telemetry values is so highly dependent on where in the ADC measurement range we are?

Is the recommendation to make sure if we want decent telemetry, we have to make sure to be in the upper half of the ADC measurement range?

We have low current requirements, but would like to cover a wider range of currents for measurement. If the lower ADC measurement range is basically not usable, that makes it difficult to find a value for Rsense that will cover everything. Meaning we would have to use different resistor values for different products.

  • Hi Sean,

    I will check and get back on this.

    Regards

    Kunal Goel

  • Hi Sean,

    Really sorry for delayed reply. Accuracy expected is shown below. It will degrade at lower currents because of lower VIN-VSENSE. At lower VIN-VSENSE, the offset of sense amplifier will dominate and degrade accuracy. 

    Regards

    Kunal Goel

  • Hi Kunal,

    I saw this in the datasheet, but it does not match with what I am seeing in real life. As I showed in my diagram, for a voltage of about 7mV, what I see in the EVK is displayed in my screenshot. So this is far, far away from +/- 6% accuracy from the datasheet that I would expect at 7mW.

    The deviations I see are more than +/- 50%, that is what I don't understand. And I see this on the EVK, just with Rsense replaced by a bigger value, using an electronic load that will draw a constant current. Since I see this on the EVK, it cannot be an issue of our specific hardware design. And since I see this with the official TI GUI, it can also not be an issue of my readout and calculation software.

    So either I must be doing something wrong, then, or misunderstand how the chip works.

    In our application, +/- 10% accuracy would be totally OK, doesn't have to be any better than that, but currently I do not have a usage scenario where I can get even close to 10%, in most cases I am like 50% off and then the measurement is almost useless.

    FWIW, I am using an AIM LD300 electronic load. The device is a bit old, bus has served us well over the years. I will check with a scope tomorrow if maybe that load's regulation is off and the actual current is not stable, that would be the only explanation I have left.

  • Hi Sean

    Yes it would be helpful if you can check how actual current is.

    Regards 

    Kunal Goel