Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220: TX/RX pins swapping

Part Number: HD3SS3220

Tool/software:

Hi,
We have done swapping of TX and RX differential pins in output of MUX towards USB- typeC connector as shown in below figure.

Will it work, even if I swap the pins or CC logic need to be changed?

  • Hi,

    You will need to swap the CC1 and CC2 pin connections between the HD3SS3220 and the USB-C connector. Our device uses the CC1/CC2 lines to determine which orientation the Type-C cable is in. Since you are essentially swapping the orientation (TX1/RX1 <--> TX2/RX2) you will need to swap CC1 and CC2 as well.

    Best,

    Shane