This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A47: PLL & CB Power Supply Design verification

Part Number: TPS7A47

Tool/software:

Hi Team

Please help to review the design below and provide your feedback.

1) 3V3_PLL

Part number: TPS7A4701RGW

Input Voltage: 6.5V

Output Voltage: 3.3V

Load current: 377mA

Application: PLL Input

2) 2V5_CB

Part number: TPS7A4701RGW

Input Voltage: 6.5V

Output Voltage: 2.5V

Load current: 607mA

Application: PLL Clock Buffer Input

Thank in Advance,

Regards

Haritha

  • Hi Haritha,

    For 1), I calculate the output voltage to be set to 1.4V + 1.6V + 0.4V + 0.2V + 0.1V = 3.7V. They need to remove the connection to pin 10 (0P4V) for a 3.3V output. I want to also note that the startup time with CNR = 1uF is about 50ms. This isn't an issue, just want to make sure they understand this. 

    For 2), I calculate the output voltage to be set to 1.4V + 1.6V + 0.8V + 0.2V + 0.1V = 4.1V. They need to remove the connection to pin 8 (1P6V) for a 2.5V output. Same note for the startup time. 

    Everything else looks good.

    Regards,

    Nick

  • Hi Nick,

    Thanks for the quick reply.

    1)Resistor R618(DNP) which is connected to pin 10 of IC will not populate in PCB (BOM Quantity is 0)

    2)same with second IC - Resistor R615(DNP) which is connected to pin 8 of IC will not populate in PCB (BOM Quantity is 0)

    We need startup time should be less than 5ms, so it ok CNR if we change to 0.1uF??

    Thanks & Regards

    Haritha

  • Hi Haritha,

    The datasheet has the equation to calculate the startup time. With 100nF, the typical startup time for the 3.7V output is 10^5 * 100nF * ln((3.7 + 5)/5) = 5.5ms, and for the 4.1V output is 10^5 * 100nF * ln((4.1 + 5)/5) = 6ms. You will need to use a smaller CNR and note that this is a typical startup so you will want to add margin as well. 

    Regards,

    Nick