Other Parts Discussed in Thread: PMP40909
Tool/software:
Hello,
we build up the reference design https://www.ti.com/tool/PMP40909 to do some tests before we use it in our design. We had quite trouble to bring it up which had nothing to do with the usage of two TPS61288 in parallel. During the first power up we considered the usual precautions: The output was unloaded, the power source was current limited to 100mA. The input voltage was set to 5V, the output voltage to 12V. We only used one of the two TPS61288 on the board for the first tests. But directly during power the TPS61288 died. Before we powered the board, we could measure Vf of the body diode between the SW pin and the VOUT pin. After the powering the board there where zero ohm between SW and VOUT. After replacing the defective TPS61288 we could reproduce this behaviour. Also with another board same happened. To make it short: The root cause on board level was, that 100pF instead of 100nF whre mounted for the boost capacitor.
Now everything works as expected. But we can absolutely not explain ourself why this can destroy the TPS61288 in such way. Do you have any idea what could went wrong here? From our perpective none of the device specifications where violated. Neither the voltage at any of the pins, nor any current limits. When I took waveforms at the switch and boost pin, the voltage was never above VIN (5V). Maybe there is a mechanism, that in this case VGS of the HS MOSFET will exceed its limits?
Many thanks and best regards,
Christian