Part Number: BQ25180
Tool/software:
Our battery powered device (charging with USB) contains a BQ25180. The device can shut itself down by sending the command for ship mode to the BQ25180 which then shuts down everything else. Wake-up is done by pushbutton or USB power.
Generally it works fine on several devices (about 400). Just in very rare cases the device only wakes up from USB power. Even if it is shut down and started again several times (sending the command for ship mode to the BQ25180, waking up with USB) the problem remains. After removing and inserting the battery, everything works normally again.
For some reason the BQ25180 does not wake up from ship mode anymore in these rare cases until the battery is removed/inserted.
Command for software reset did not change anything.
Command for hardware reset worked fine on two devices. On another device the ship mode does not work anymore at all after hardware reset. We did not remove the battery yet on that device. Probably everything would work after removing/inserting the battery.
We did not notice any difference in the status registers between normal working devices and devices that don't wake up from ship mode.
Is there any reason why the BQ25180 acts like this? How to get it working normally again?