This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220: Mux or Re-driver

Part Number: HD3SS3220
Other Parts Discussed in Thread: TUSB522P

Tool/software:

I have used Mux and calculated insertion loss for entire channel. Have the following components on the entire path for DFP mode USB3.1 gen-2 5 Gbps.

Processor module-- connector-- mating connector-- Mux-- C-type connector

3" length on processor module+ connector/ mating connector-- 5.5" till Mux-- 2" till C type connector.

when I have calculated the insertion loss around -11dB.

Would you suggest to go with redriver or any other solution?

and what is the targeted insertion loss from processor to type-C connector? and if we want to use cable to connect flash drive will it work?