Part Number: TPS3825
Tool/software:
Dear SirMadam,
My end customer is using TPS3825-33DBVT for voltage monitor (meter function), They are doing reliability test on thier end product and when temperature reach -30 degc, they noticed the unit keep reseting the MCU.
The picture on the right is their connection diagram which the unit suppose to generate reset when VDD fall below 2.93V. I saw their circuit has some extra resistors in front of /MR pin, I would like to know will this causing this failure issue.
According to application section of datasheet, the connection diagram is as follow:


Hope to get some advise. thx
Best Regards,
KPK