Part Number: TPS63060
Tool/software:
Hello,
I am an FAE at a distributor that handles TI products.
I received the following question from a customer.
I would like to ask about the "PG output low voltage" listed on the datasheet.
Under TEST CONDITIONS it says Ipgl=10uA.
(Question 1)
Is this 10uA a value determined by the pull-up resistor?
(Question 2)
If the answer to question 1 is "yes", what is the maximum voltage of "PG output low voltage" for example Ipgl=300uA?
It says that MAX=0.4V for 10uA, so I would like to know what the MAX value is for 300uA.
Best regards,