Tool/software:
Hello Expert
I am using TPS92515 IC for my project. With 24V input voltage, can I use it to drive 3.3V LED with max current 2A without any problem? Can I use additional filters like Pi filter at input to reduce noise, can expert share with me some suitable noise filter ?
Operating conditions:
Vin = 24V
LED Vf = 3.3 (typical )
LED forward current: 1A ( typical) / 2A ( max )
Thanks and regards !