This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27524: Changes in VDD during operation

Part Number: UCC27524
Other Parts Discussed in Thread: UCC27624

Tool/software:

Hi team,

I am considering using UCC27524 to drive a pulse transformer in a PSFB circuit.

At startup, VDD is 12V, but after PSFB starts, it rises to 18V.

Is it okay to use it like this?

Since SiC is used, the gate voltage needs to be increased.

Best regards,