Other Parts Discussed in Thread: UCC28630
Tool/software:
Hi Team, A customer of mine is facing the following problem with the low power startup .
I have been designing a Switching Supply based on the UCC28631 and we are looking at going into production early next year. Recently I have noticed a potential issue and am wondering if Texas Instruments has a solution.
Due to the low standby power requirements coming into effect next year the SNT has been designed with this in mind and has a <200mW standby at 230Vac and with the target application connected it is a little over 400mW.
In certain circumstances the IC will actually lock out and not restart. This occurs sometimes when the AC power is turned off briefly. To get the IC to restart you have to disconnect the AC input and wait for the bulk capacitor to drain completely which takes quite a while with the low standby power.
Has this issue been noticed before and is there an easy solution?
Could you help with the same?
Best,
Maitriya