Part Number: LM25145
Other Parts Discussed in Thread: LM5146, LM5146-Q1
Tool/software:
I am using the LM25145 in my design. My input voltage range is 16V-26V. The typical load current will be around 4-8A, and the maximum current will be around 12A.
I am using feedback resistors of 22K and 12K to achieve a 2.26V output voltage. I have used the LM25145 quickstart file to check the compensation values. I tried input voltages from 14V to 24V, and the output voltage is always fixed at 2.6V. However, when I set Vin to 10V or 12V, the output voltage is 2.3V. I did not connect the load; I just want to check the output voltage. Can you guide me on where the problem might be? I want to get a 2.3V output voltage when the supply voltage is in the range of 16-24V.