This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77216: Component question

Part Number: BQ77216
Other Parts Discussed in Thread: BQ77307, BQ76952

Tool/software:

Hello,

I am using the BQ7721611 component.

It has specific UV and OV limits.

Do you have this type of IC with at least 15 cells that i can control the UV and OV limits using external resistors?

  • Hello Maor,

    No, unfortunately we do not have such a device. The closest protector that could potentially do this would be the BQ77307, which has programmable protections. But it requires an MCU in order to change the protection thresholds. 

    An alternative would also be the BQ76952, which is a monitor and protector up-to 16 cells and is highly configurable. This device could be OTP'd by the customer with any custom settings.

    Best Regards,

    Luis Hernandez Salomon