Part Number: UCC21520
Other Parts Discussed in Thread: UCC21550
Tool/software:
Hello, can i use UCC21520 to drive HV(600V) MOS? If it cannot work, could you pls promote a suitable device? Thanks a lot!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Woney,
Yes, UCC21520 is capable of driving a 600V HV MOSFET.
I recommend to look into the new generation refresh of this product: UCC21550
UCC21550 is a refresh of UCC21520 with improved robustness and better cost structure.
Please feel free to ask any additional questions below!
Regards,
Hiroki
Hi Hiroki, thanks a lot for your answer. UCC215220 has two outputs, can each output be able to drive 3 paralleled 650V MOS (part number IPW60R037P7)? If not, can UCC21550 or other devices can make it? Appreciate!
Hi Woney,
Yes, both drivers will be able to drive 3 MOSFETs in parallel. However this depends on a number of factors.
Here is a calculator you can use to check this with the customer's system: 7725.Gate Driver Max Frequency Calculator.xlsx
As long as the frequency is within the max frequency, there should be no issues.
Regards,
Hiroki