Other Parts Discussed in Thread: CSD25480F3, CSD25483F4
Tool/software:
Hello
I need your help
I'm designing a pcb board and it needs to have the ability to switch between 2 devices.
General characteristics:
DC voltage
Power - 12v 0.5A
Power - 9V 0.66A
Power - 5v 1.2A
Total power normally works 6 watts
Control through a microcontroller
Logic
if input 0 - device 1 enable Power
device 2 disable Power
if input 1 - device 1 disable Power
device 2 enable Power
Is there anything similar IC in functionality from TI?