Other Parts Discussed in Thread: UC2842
Tool/software:
Hi TI team,
i am working on UCC28C55-Q1 and I have query regarding how to calculate Rss,Css based on soft start time .It is mentioned in the datasheet as 1mA of the Error amplifier output current will charge the Css capacitor thought the PNP transistor.
By taking 1mA current metioned in the datasheet below and using formula,
Css * Vcomp =i *tss
By taking Vcomp pin voltage is 5V and reuired soft start time of 20ms ,can i calculate Css * Vcomp =i *tss ==> Css= (1mA* 20mA)/ 5V = => 4uF.Is this correct??
It will not charge from Vref??

Because in the Ti forum for UC2842 soft start time,it was metioned as ,

can i use like above picture to calcualte the soft start time as Vref will charge the Css capacitor .Got confused after seeing this post whether Vref will charge the Css or E/A output (Comp pin) through PNP transistor will charge the Css capacitor.
Can you clarify this and kindly suggest correct way to calculate the soft start time with Rssa and Css.
Thanks,