Other Parts Discussed in Thread: TPS61022
Tool/software:
Is TPS61178 suitable for the following designs?
Vin = 3V to 4.2V
Vout = 5V/2.5A
Have any TPS61178 design calculate tools?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I attach files on the attachment.
The conditions I use dynamic electronic load are: 0.75A~2.5A, 10ms, 2.5A/us.
I hope to reduce the output voltage ripple by 5V +/- 5% when doing Transient Test.
Please tell me how can I improve it?
Hi,
The Webench has output capacitors with 3X22uF/10V 1206, the efficitive is about 30uF totally.
In schematic is 2X22uF/6.3V 0603, which is only 13uF totally.
As a result, in webench design, the cross frequency is about 3k and in schematic it is much higher like 10k;
it is hard to increase the cross frequency as it is quite high and easily to be unstable.
It will be better to improve the output capacitance and increase the Rcomp at meantime that we can improve the load response.
Best Regards,
Fergus
Please use the formular to estimate the transient.
The Cout and fbw directly influence the transient response.
Also, the stage loop gain and compensation loop can be gained by(refer to the datasheet):
then you can see find the fbw accordingly.
Best Regards,
Fergus