This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5143: I want to use LM5143 to design a dual-phase 24V to 12V, 20A buck circuit, can you help me to look at my problem

Part Number: LM5143
Other Parts Discussed in Thread: LM25143

Tool/software:

Good afternoon,
I use LM5143 to carry out a 24V to 12V dual-phase BUCK circuit, but it can't work, and the phenomenon is strange, the output is only 0.5V, and the SW has no waveform. The following is my schematic diagram, which is completely designed according to WEBENCH

Then this is the result of WEBENCH

Please help me check, thank you very much