Other Parts Discussed in Thread: TPS61033
Tool/software:
Hi
I am evaluating the EVB(TPS61033EVM-105).
I set the Out Voltage and Out Current limit of DC Power Supply as below.
The EVB load is 62.5ohms(80mA).
I think the out power of the DC power Supply(when setting 150mA) has already exceeded the power that need 0.45W.
The efficiency is about 88%.
But the EVB can normal output 5V 80mA until setting the the Out Voltage and Out Current limit of DC Power Supply to 5V 300mA or 4.25V 300mA.
Could you tell me why?
Thanks and Best Regards,
Chunli Liang