This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25125: Inductor selection

Part Number: BQ25125

Tool/software:

Due to space constraints I have to use a very small SMD inductor on the SW pin.

The datasheet recommends to use a 2.2µH inductor but these are not available in sizes smaller than 0603.

I found a small 1.5µH inductor:  TDK PLE856CCA1R5M-1PT00 but I am unsure if this will work.

It is rated as:


- 1.5μH ±20% at 1MHz

- Isat 330mA (max), 400mA (typ)

- DCR 520mR (max), 450mR (typ)

My system uses

- 5V USB-input

- 1,8V SYS 

- 1,8V LDO

- Typical current: ~ 4-50mA but I want to lay it out for peaks up to 150mA

In the "SLURAY9 — BQ25125 Setup Guide Tool" I can change the inductor  to 1.5µA and with ISYS(Max) 150mA the Pk-Pk Inductor Ripple Current increases from 261,8mA to 384mA and Maximum Inductor Current from 280,9,9mA to 342mA.


Can I use this 1.5µH inductor?

Do I have to change other values e.g. the output capacitor (currently 10µF).

Will the efficiency drop a lot compared to the 2.2µH?

Is there anything else to consider when changing the inductor?

  • Hi,

    Yes, a 1.5uH inductor can work with this device at lower current consumption.

    The output capacitor can remain the same value.

    Efficiency may be affected. One major component characteristic to take into consideration is DCR and how it compares to alternative selected inductors.

    Saturation current, maximum inductor current, and output ripple are all possible effects to take into consideration when selecting inductor. 

    Best Regards,

    Juan Ospina