Part Number: BQ25125
Tool/software:
I want to use Vsys with 1.8V and LDO with 1.8V which seems to be the default setting for BQ25125 as written in the device comparison table in the datasheet.
I have some questions:
1. The typical application example connects SYS and VINLS. The table "Electrical characteristics -> LS/LDO Output" says 2.2V are required on VINLS for LDO operarion.
- Does it work when SYS and VINLS are connected to get 1.8V on LDO?
2. Chapter 9.3.21 says "If the output of the LDO is less than the programmed V(SYS) voltage, connect VINLS to SYS. If the output of the LDO is greater than the programmed VSYS voltage, connect VINLS to PMID."
- In our situation, VLDO and VSYS are equal. Should I connect VINLS to SYS or PMID?
3. VINLS does not have a capacitor in the typical application but the datasheet says "Connect 1 µF of effective ceramic capacitance from this pin to GND".
- Do I need the capacitor?
- Is it also required even when PMID is connected to VINLS? PMID already has a 4,7µF capacitor.