Part Number: LM3409-Q1
Other Parts Discussed in Thread: LM3409HV-Q1
Tool/software:
Question: LM3409HV-Q1 is used to drive three RGB lights. The front-end of this circuit is connected to a 9V~15V power supply, and the output of the chip is connected to the RGB lights. When the VADJ is fixed, adjusting the input voltage (for example, when it is currently 12V and adjusted to 10V) will change the color of the lights. Will the input voltage change of this device affect the output voltage or current change? The chip is driven by a constant current, and if the voltage of VIN is adjusted normally, VOUT should be stable and unchanged. Is there a design error on my part?
The above diagram is a link to the specifications, which were drawn according to page 12 of the specification sheet. However, the RGB three lights are connected in parallel, and the common anode of the three LEDs is connected to VOUT. The cathodes of the LEDs are controlled by MOS transistors and grounded.
Many Thanks for your support.