Part Number: BQ24725AEVM-710
Tool/software:
Hello,
I'm evaluating the BQ24725AEVM-710 for charging one cell Ni-MH battery.
The input Voltage is 5V (I have modified the ACDET resistor accordingly) and the SYSTEM output is not used.
When setting the output voltage at 1500mV and current at 1024mA, I'm still seeing roughly 500mA maximum current.
I noticed when rising the output voltage above 2500mV the maximum output current limit start to work properly.
I think I've checked everything but I still haven't found the reason why it's not able to deliver more than 500mA at 1500mV output.
Could you please check if I've missed something?
I can share some waveforms if necessary.
Thank you very much!