Other Parts Discussed in Thread: BQ25895, BQ2980
Tool/software:
Hello,
We are looking for a Li cell protection where with the following specs:
OV cut off @ 4.2V - we will perform CV charging at 4.15V
UV cut off @ 3.2V preferable, 2.8V lowest.
The closest I can find for this is with BQ2982 series, where I need to use BQ298218 (OV at 4.2V) for OV detection and BQ298009 or BQ298010 (UV of 2.9V) for UV detection. Would this be possible to use two of BQ298x series, one for OV and one for the UV? Or is there any other option available?
Regards, Prithvi