Tool/software:
Hey, I bought the Adafruit Solar charger for testing the BQ24074 IC and I had A LOT of problems with it. Now I am using the EVM Board to get my setting right for the PCB print. Finally I am nearly done. But there are still some questions in my head to make sure i have understood the BQ24074 IC.
I am planning to charge my Lipo with a standard Smartphone charger. The Lipo should power a Boost converter which needs 0,5 A (maybe 0,6 for a short time (ca, 0.5 sec)). I also want to be able to use a powerbank to increase the lifetime of my device. In this situation the charging is not necessary but would be nice to have.
I tested the ILIM Mode with I_Lim = 1,460 A and a charging current of I_Charge = 0,,887. I measured the the voltage of R_iset to calculate the charging current over time. Looks beautiful (see picture below)! BUT: I Set my power supply to 5V i observed that the current output is the same or even more as the charging current. It follows that more than 0.2 Watt are used somewhere in the BQ24074EVM. But where? Is it heat? Is it normal? Any suggestions to reduce this "power loss"? I need the device to be very safe when it comes to heat.

Another question, but I think it goes in the same direction:
In the datasheet FIG 8-12 (see below) Vin is 6V and the mode is USB500, which means a maximum power supply of 3 watts. The graph shows 1 amp at 4V. How can 4 watts be supplied? I have the feeling my math is broken:)

Last question:) The Adafruit Solar Charger uses a Diode (SK34D) at the Power Bus of the USB-Input. In my test the voltage drop caused a lot of problem (at least i think the this is the reason:). Do you think i can safely implement a USB-C power supply without using a diode?

I´m happy about every answer, every tip and every comment :)
Best,
Chris