Tool/software:
Hi,
I am planning to use BQ7790518 for charging OV protection of a 8S battery pack. In the EVM, I have tested the charging scenario and made one of the CELL voltages greater than 4.2V. The circuit is shown below. My doubt is when the CHG MOSFET is OFF, there is still the battery voltage - the antiparallel diode voltage of the CHG MOSFET is seen, however the current is zero. Is it because of the MOSFET package? According to my understanding, after cutting off the voltage across the charger terminal (PACK+/PACK-) should have been OL means open.