This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74502H-Q1: Feasibility of LM74502H-Q1 for use in motor output cutoff application

Part Number: LM74502H-Q1
Other Parts Discussed in Thread: LM74800-Q1

Tool/software:

Hi,

In a specific motor drive related automotive application, I need back-to-back MoSFET to prevent back EMF when battery supply to the drive is disconnected. Please see the figure below.

I am planning to use N-channel MoSFETs to realize this. I need a suitable high side driver to control these switches. The motor is rated for 12V.I have found the part LM74502H-Q1 and needs confirmation if this supports the purpose. Or else can you please support in selecting a suitable driver for the N channel mosfets connected back to back.