This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCR022405

Other Parts Discussed in Thread: DCR022405

Hallo Tom,

is it possible to connect the capacitor such as 47 uF at the output of DCR022405? Is there any maximum limitation in installing output capacitor?

We have installed input capacitor >10uF for each DCP/DCR elements.

Must be used additional input elements if we use parallel 3 x  DCR022405 and 5 x DCP022415 (summary input capacitor >150 uF).

Thanks