Other Parts Discussed in Thread: EV2400, BQSTUDIO
Tool/software:
I have two EVM boards. The original version with embedded EV2400 module, and the smaller version that requires a separate EV2400 interface. The issue I am having is the same foe both versions.
The first issue is that BQ Studio does not Auto Detect the device, so I have to manually select the "Gauge" type, then select the correct fuel gauge part. It does not matter if I select 1561_0_04-bq27z561 or 1561_2_01-bq27z561R2, when I click OK, I get the following warning message:
If I click OK, then the connection to the device on the EVM is unreliable. I am unable to successfully write a golden image (srec or bq.fs). Unseal commands work occasionally, and the device randomly disconnects.
Can I get some guidance on how to make this setup work? I am stuck until I can resolve this issue.
Cheers
Jason