Other Parts Discussed in Thread: UCC28730, UCC28610, UCC28631
Tool/software:
Hi,
I need to design a flyback converter with 2 isolated outputs (12V 10mA, 6V 350mA).
Input 18V - 70Vdc
The most important requirement is the no-load consumption, preferably < 10mW.
To me this indicates a PSR converter where there is no optocoupler current.
UCC28910 looks good but only mentions a possible no-load of < 30mW.
Price is off course also a major factor.
Does TI have another more suitable solution?