Part Number: LM25149-Q1
Other Parts Discussed in Thread: LM25149, LM25148
Tool/software:
Hello Team
We want to use LM25149-Q1 for Automotive controller power. We designed the circuit with information obtained using WEBENCH.
We designed it to be able to output 5V voltage at 12V input and output up to 20A current, but we would like to confirm the design contents regarding the operating frequency setting, EMI filter, and AGND configuration.
1. The input power is supplied by the battery. So, for space efficiency, the EMI active filter at the input stage was not used, and only the SSC was activated. If it is more efficient to combine the SSC operation of LM25149 with the EMI active filter operation, would it be better to add it?
I have attached the content output from WEBENCH regarding this content. Please give me your opinion.
2. WEBENCH recommended a design that sets the frequency of LM25149 to 743kHz. Is this a value that considers the output power and current compared to the input? If not, is there a recommended value?
3. Since no EMI active filter was used, the grounding other than PGND was treated as AGND. Please review the attached circuit diagram.
I look forward to your reply.
Thank you.