Tool/software:
Hi all,
1) Referring to Figure 18 in the datasheet, I am considering changing the GND of LMG1210 to the source of the Lowside FET.
I think I can avoid potential fluctuation of the GND due to sense resistance.
In EVM, current detection is done at the end of the inductor, so I think it is possible.
Can I have the Gerber data of EVM and the pattern circuit diagram for reference?
2) In the circuit diagram of EVM, R3 and R10 are designed to be 0Ω, but is it correct to use the gate resistor?
Best Regards,
Ryusuke