This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-PSFB-DCDC: Full-bridge isolated DCDC solution

Guru 12410 points
Part Number: TIDM-PSFB-DCDC


Tool/software:

Hi,

Is there a full-bridge isolated DCDC solution that can be implemented under the above conditions with both the primary and secondary sides full-bridge?

- Input 40V-100V
- Output 25-50V

Probably a solution combining C2000. The purpose is to increase efficiency in the circuit.

Thanks,

Conor