This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: BQ25703A

Part Number: BQ25703A
Other Parts Discussed in Thread: BQ25703

Tool/software:

Dears,

Use bq25703 charging chip and cw2015 power meter. During use, it was found that the charger still has voltage (fast charging 12V voltage) and a small current (0.16A) when charged to 100%. Is there a plan to turn off the charging function at 100% to prevent overcharging?? If so, how can it be implemented?

Thanks