Other Parts Discussed in Thread: TPS61288
Tool/software:
Hello.
This is Kwonjoon Lee from South Korea.
I would like to ask about a discharging operation of the TPS7A4901.
(Detailed Situation)
1. The VIN of my TPS7A4901 is connected to the output of TPS61288 (boost converter)
2. The EN of my TPS7A4901 is connected to the VIN.
(Questions)
1. In the case that a voltage of the VIN of my TPS7A4901 is rapidly decreased by
the TPS61288's disabling (the EN pin of the TPS61288 = Low), and
the VIN of the TPS7A4901 is lower than the VOUT of the TPS7A4901,
what is a main discharge path of my TPS7A4901's output?
I think that I have the following three candidates for discharging path:
1) a power clamp diode (or a PN diode of the internal PMOS pass transistor) between the VOUT and the VIN of my TPS7A4901
(what is the maximum allowable current?)
2) the feedback resistances of my TPS7A4901 (a few tens of kohm)
3) a load of my TPS7A4901's output (light load)
2. I would like to ask the discharging operation of the TPS7A4901 (and TPS61288) is modeled in the SPICE model for PSpice for TI?
Best regards,
Kwonjoon Lee