This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825-SP: Fixed duty open loop push-pull

Part Number: UC1825-SP
Other Parts Discussed in Thread: TIDA-00181, LM5030

Tool/software:

Hello, I would like to design an open loop fixed duty push-pull converter (no output inductor) using UC1825-SP.

Something like described in TIDA-00181 for LM5030.

The target is 12V output at 100mA starting from a 12V input. Are there any drawbacks?

Is there an application note with any suggestions ?

Thanks. Regards, Ottavio Di Sauro