This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563203: TI Recommendation

Part Number: TPS563203


Tool/software:

Hello:

Customer is inquiriing about TI‘s Buck chip. below is requirement. I can't find suitable chip on TI’s website, Please help recommand,Thanks!!!

1. The input range requires 2.7V~32V, the output voltage is 4V, and the maximum output current is 5A;

2. Buck voltage reducing chip with bypass function;

3. Low MOS Rdson, excellent heat dissipation performance;

4. Equipped with OVP protection, over temperature protection, automatic PFM/PWM regulation, etc;

5. Prioritize QFN packaging.


笔记