This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62912: Synchronize the TPS6291x by a source which is powered by the TPS6291x's output voltage.

Part Number: TPS62912


Tool/software:

We tested the TPS62912 in your evaluation board and are really happy with it.

However, our design needs the TPS62912 to be synchronised by a clock source which is powered by the output of the TPS62912.

Is there a simple way to use the combined EN/SYNCH pin to make the desired approach feasible?

Input 12V goes to the TPS62912 which generates 5V. This 5V supplies an OCXO. Its output (2MHZ) synchronises the TPS62912.

Other DCDC-converters have separate SYNCH and EN inputs. Thus the implementation of the above design is easy.

Any help would be really appreciated!

  • Dear Sir, 

    You can refer to datasheet 7.3.2 and 7.3.3 for the details about how to configure EN/SYNC.

    The device is enabled by pulling the EN/SYNC pin high, and has an accurate rising threshold voltage of typically 1.01 V. Once the device is enabled, the operation mode is set by the configuration of the S-CONF pin. This occurs during the device start-up delay time tdelay. Once tdelay expires, the internal soft-start circuitry ramps up the output voltage over the soft-start time set by the CNR/SS capacitor. The start-up delay time tdelay varies depending on the selected S-CONF value. It is shortest with smaller S-CONF resistors. The EN/SYNC pin has an active pulldown resistor RPD. This prevents an uncontrolled start-up of the device, in case the EN/SYNC pin cannot be driven to a low level. The pulldown resistor is disconnected after start-up. With EN set to a low level, the device enters shutdown and the pulldown resistor is activated again.

    The EN/SYNC pin is also used for device synchronization. Once a clock signal is applied to this pin, the device is enabled and reads the configuration of the S-CONF pin. The external clock frequency must be within the clock synchronization frequency range set by the S-CONF pin. When the clock signal changes from a clock to a static high, then the device switches from external clock to internal clock. To shutdown the device when using an external clock, EN/SYNC must go low for at least 10 µs.

    BRs

    Lucia

  • Dear Lucia

    Thank you very much for the quick answer.

    Exact these chapters in the data sheet led me to the question.

    Applying 12V needs the EN/SYNC pin to be high to start the TPS62912. But because the OCXO ist not supplied with +5V its output signal is 0. So, I need to enable the TPS62912 somehow with the 12V and later, when the clock signal from the OCXO is available, I have to switch over to the clock signal.

    Sure, there are cumbersome ways to accomplish that. But I hope you have a smart solution to fulfill this desired behavior. Because if the EN and SYNC functionality were separated the design would be easy.

  • Hi Konrad,

    Thanks for your feedback. But as EN/SYNC is not separate, looks like no other smarter way for TPS62912 based on your application in my mind. Thank you!

    BRs

    Lucia

  • Hello Lucia

    Thank you very much for the confirmation.


    With best wishes
    Konrad