Tool/software:
Hello,
I have some questions during validation TPS61094 via TPS61094 EVB.
Test conditions:
Vin = 5.2V (makes sure Vin > target Vout+0.1V)
Vout = 5V
Charge current = 300mA
Charge voltage = 5.1V
Load current = 1A.
1. How to forecast the efficiency load current above 0.5A? We need scope of load current from 0.5A to 1.5A ,but only record to 0.5A in datasheet.

2. The range of current limit from 1.7 to 2.6A. It's look like decided by it's made so may I might be able to change the current limit by resistor dividing?
Or I should set the current limit at 1.7A in my design.

3. The following is captured by oscilloscope, the pic. is mark 1 and 2 separately

3.1 At the mark 1. My sequence is load 1A in then turn mode to auto buck and boost, turn off Vin. When turn off Vin, Vin、Vout and Vsup all has ripples that look unusual, what is cause it?
If it is normal how could I reduce it ?

3.2 After turn off Vin, then Vsup is decrease to 2.26V then Vout is shutdown.
According to the document, UVLO is Vin and Vsup both below 1.7V, but in my test Vsup still above 2.2V , what kind of mechanism shutdown the Vout?

Thanks!
Jensen