This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79612-Q1: One single balancing resistor instead of 2

Part Number: BQ79612-Q1


Tool/software:

Hello,

Would the balancing of the battery cell work if I replace the balancing resistors 2xRCB=10 by 1xRCB=20? I understand the internal CBFET would be biased differently in this case.

Thank you,

Abbas

  • Hi Abbas,

    Are you referring to our 2 Rcb resistors in parallel in our EVM schematic? If this is the case, keep in mind that the parallel resistors bring Rcb to 5 ohms. Replacing both resistors with a single 20 ohm resistor brings significantly increases Rcb.

    In order to calculate the cell balancing resistance, you need to do:

    Rcb_total = 2(Rcb) + Rcbfet

    Where Rcbfet is 1.5 ohms.

    With this you can calculate your cell balancing current with V = IR, where V is your cell voltage and R is the Rcb_total you just calculated.

    With a larger Rcb, you will have lower cell balancing current. But yes, this is okay if it is the goal.

    Best,

    Zachary

  • Hi Zachary,

    No it's not what I meant.

    Let me say it differently: if I remove one of the two Rcb I understand that the current will increase for sure but would the balancing still work with only one Rcb ? Would this not disturb the biasing of the internal Mosfet QCB?

    Rcb_total remains at the same value but I increase one Rcb and remove the other one: Rcb_total = 2(Rcb_a) + Rcbfet= Rcb_b + Rcbfet

    In other words, on the PCB I use one resistor instead of 2 but keep same Rcb_total.

    BR, Abbas

  • Hi Abbas,

    Could you kindly provide a diagram or simple drawing for which resistors you are planning on removing and which resistors you would like the change?

    Best,

    Zachary

  • Hi Abbas, 

    Yes, it is totally fine to replace the CB resistors, this won't effect the MOSFTS. Although from what I understand you are increasing the resistance from 10 ohms to 20 ohms, this won't keep the CB current the same.

    Best,

    Zachary