Other Parts Discussed in Thread: BQ25756
Tool/software:
Hello,
We use the bq76952 as a monitor in parallel path configuration and the bq25756 charger as shown in the sketch below:

We control the discharge and charge FETs with the DFETOFF and CFETOFF pins. When the discharge path is enabled(DFETOFF pin enabled) the device enters sleep mode if no load is connected to PACK+. This is as expected.
But the device does not enter sleep mode if the discharge path is disabled. The WAKE bit is set then all the time. Then it would make even more sense for the monitor to go into sleep mode. How can we fix that problem? Or what can cause that?
We do not have a blocking diode or blocking FET behind the charge FET and therefore the PACK pin is always high. Does this cause the behavior we see?
Here are some of our register settings:



What can cause that and how can we achieve sleep mode also with disabled discharge path?
Thank you in advance
Lukas