This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS723: TPS72301

Part Number: TPS723


Tool/software:

I want ot drive the enable pin from a 1.8V output. Acc to the datasheet the min enable voltage VEN(HI) is 1.5V. It says nothing about max voltage.

Is 1.8V at the enable input guaranteed to enable the device?

  • Hi Kalle,

    Yes, the way to interpret the EN spec is that any voltage above 1.5V (min) enables the device, and any voltage below 0.4V (max) shuts off the device. So, 1.8V is guaranteed to turn on the device.

    Regards,

    Nick