This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61041: Suitable DC/DC Boost for powering OP amps in audio application?

Part Number: TPS61041
Other Parts Discussed in Thread: TPS61377, OPA2990, OPA1678, TPS61170, TLV61047, TPS61372

Tool/software:

Hello,

I am looking for Boost converter for powering OP amps in audio application.

Parameters requirements. Maybe you will advice me someone better.

1. need to boost 5v to +12V - also I want to use charge pump circuit for creating the -12V rail.

2. Is constant switching frequency (PWM mode) better than PFM mode for audio application?

3. I am very limited with space, so small packages only like: DFN, WSON but not BGA type packages.

4. Also good price is good too.

I found only mentioned TPS61041 but it works in PFM mode and I am scared if this is good for audio (op amp). Looking for advice if I can use it and some switching noise depending on the frequency change will not be transmitted and hear in audio.

My last question - is it good to connect OP amp directly to this type of symmetric power rail? Boost + charge pump circuit? (picture for reference)

Thank you

Best regards,
Martin

  • Hi Martin,

    What's the max current needed for the OPA? I'd like to check whether the Iout is big enough to cover your application.

    2. Is constant switching frequency (PWM mode) better than PFM mode for audio application?

    PWM mode is more recommended to make both the positive and negative output stable.

    I found only mentioned TPS61041 but it works in PFM mode and I am scared if this is good for audio (op amp). Looking for advice if I can use it and some switching noise depending on the frequency change will not be transmitted and hear in audio.

    Again I need the total Iout to check the work frequency. We also have device such as TPS61377, which can work in FPWM mode. 

    My last question - is it good to connect OP amp directly to this type of symmetric power rail? Boost + charge pump circuit? (picture for reference)

    It depends on the OPA you used. When the Iout is confirmed, the Vout ripple can be estimated, then you may check whether it is acceptable based on the OPA PSRR.

    Regards

    Lei

  • Hi Lei,

    Thank you for respond.

    So, I must rather find the PWM mode Boost controller.

    Iout will be about 20mA max. Or maybe lower? What do you think? According to my schematic below.

    Thanks for recommendation TPS61377 but it is quite overkill. So much not necessary pins. Some another similar to TPS61041?

    For now, I have in schematic placed this OP amp - OPA2990 WSON 2x2. And also this one looks good OPA1678, but package is bigger.  But you can recommend me another. UPDATE: I will use OPA1678. I made space on PCB.

    This my my audio application. There are connected signals from XLR connector. 

    Thanks
    Regards,
    Martin

  • Hi Lei,

    Regarding to Boost converters..

    I found these two: TPS61170 or LM2735XSD. I will rather use TPS61170 because it is smaller. Could you help me to choose right inductor value for application with OPA?

  • Hi Martin,

    For TPS61170 in your +/- 12V application, a 10μH inductor will be a good choice.

    Iout will be about 20mA max. Or maybe lower? What do you think? According to my schematic below.

    The +/- 12V output are used for the power of OPA, right? From the schematic I think the Iout should be small.

    Thanks for recommendation TPS61377 but it is quite overkill. So much not necessary pins. Some another similar to TPS61041?

    As my calculation, when 10μH inductor is used for TPS61170, it works in PWM mode when the total Iout (from both +/- 12V) is greater than 50mA. So, if the total Iout is 20mA, TPS61170 should still work in PFM mode.

    There is a more recommended device for your application, the new pre-released device TLV61047, which is in SOT23 package with 2.9mm x 1.6mm. Although the size is bigger than TPS61170, the advantage  of TLV61047 is that it works in quasi-constant fixed frequency (~1.6MHz) even in DCM mode when the load is light, for example, Vin = 5V, Vout =12V, Iout = 5mA.

    The datasheet should be available on website just these days. 

    Regards

    Lei

  • Hi Lei, 

    Thanks for suggested boost controller, but SOT-23 is so big for my pcb. Need some DFN package.

    What do you think about to use 100uH inductor with TPS61170. Than I will be still in CCM.

      

    Regards,
    Martin

  • Hi Martin,

    100μH is too large, there should be instability issues.

    Will the TPS61372 with WCSP package be available for your application? The size is smaller than TPS61170 and it had FPWM mode.

    Regards

    Lei

  • Thanks, I will try.

  • Hi Martin,

    Thank you. Just let me know if you see any concerns.

    Regards

    Lei