Part Number: LM5146-Q1
Other Parts Discussed in Thread: CSD19531Q5A, LM5146, LM5145
Tool/software:
Hello support team,
I'm trying to build a DCDC converter and used a controller LM5146QRGYRQ1. I'm completely new to power management and this is my first attempt. I started with WEBENCH Designer and built my first prototype, which was pretty unstable, so I did some research and in the datasheet, I found Quickstart Calculator. So I tried to calculate several versions and built them and the result is that some of them are gone and some unstable. Can someone look and tell me what am I doing wrong? I attached some pics and the Quick Start calculator which I used.
High side mosfet I've used CSD19531Q5A
Low side mosfet I've used BSC037N08NS5ATMA1
Output capacitors I phisically put 13x 22µF CL21A226MAYNNNE
Input voltage should be from 25V to 51V and output voltage12.2V & max output current 20A.
Thank you for your help.
3107.Pictures.zip
LM5146-q1 quickstart_25-51Vin_12.2Vout@23A -_130kHz_V1 .xlsm