Tool/software:
Hello,
We are working on a new design with an input voltage of 24V. The input voltage range is from 9V to 36V.
To create a 24V stabilized volatge inside the product we have used a LM5176.
The power consumption of design is maximum 60W so the maximum current is 6.7A.
We have follow the design requirement based on webench design.
But we have and issue on multiple board, the output voltage is not as expected.
The output voltage varies on different board but it is between 0.7 and 2V.
We have try with the input voltage at 24.8V.
EN/UVLO pin is at 3.65V.
VINSNS pin is at 24.8V.
VCC is around 3V which is too low.
Do you have any idea to go further in debugging?
Thanks in advance,
Romuald