This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3880: LM3880MF-1AA/NOPB

Part Number: LM3880

Tool/software:

Hi, 

  Could someone please help me confirm the configuration of the LM3880MF-1AA/NOPB  when the enable pin and VCC are both +5V? I see that it is not recommended to do so but the datasheet mentions that there are a few alternative options on pg. 15-16. So, it would be great if we could have a quick discussion over the phone. Thank you so much. 

Best Regards, 

Tasneem S. Khan