Part Number: BQ24070
Tool/software:
Hi Garrett,
This is a follow up to my previous thread.
I still have the original board with the fault. Now we are bringing up pre-production units and and now I've seen this problem appear in one of those...so a red flag is started to wave in my head!
I did a detailed test yesterday and have some new info.
Some of what I saw yesterday contradicts what I reported in the previous discussion about a month ago. Let's go with this new info (I can't explain the discrepancy but it may have to do with having the battery inserted at power up of the chip or not)
To recap what the failure modes are:
- With no battery connected, the status bits indicate that the chip is in fast charge mode. The BATT pins are static and at 4.2V - not cycling as per 8.4.3.5 of the datasheet which states.
- I ran the test you suggested - I took a deeply discharged battery, ~2.3V, and had that connected to the BQ24070. The system load was not present (Switched off), and a 5V bench supply was powering the BQ24070.
The charger behaved correctly - started at a charging current of ~110ma and the status pins showed that the chip was in precharge.
At approx 2.9V battery voltage the charging current went to the desired 1A and the status pins showed the fast charge state.
All was going well until the end.
When the voltage at ISET1 was in the threshold range for turning off the charger (~250mV), it did not turn off the charging current.
The voltage at ISET1 got down below 200mV before I gave up. At that point the charging current was still ~100ma.
So my conclusion was that the mechanism to shut down the charging current based on the voltage at ISET1 was not working anymore....perhaps the circuitry at the ISET1 pin was damaged.
Questions:
We have a 0.1uF cap between BAT (Pins 5 and 6) and ISET1 as per the recommendation in 9.2.2 -
"A 0.22-μF capacitor is connected between BAT and ISET1 to improve operation at low charge currents."
Q1: Have you ever seen battery load transient voltages coupling into ISET1 through this cap?
We do have large (3-4A) current spikes coming out of the 18650 battery which may cause momentary droops in the battery voltage....which if steep enough in terms of being step changes in voltage could couple through that cap.
(Note that these high currents do not pass through the BQ24070 - we have a "high current path" from the battery in parallel with the chip).
I will be doing some lab measurements today on what the load transients may look like on the battery and will report back.
Q2: What is the impact of not using the 0.1uF cap between BAT and ISET1.

Q3 - One more thing I should mention is that in our application we always have the 5V adapter plugged in and when we need to perform an operational cycle, we switch to battery by disabling the BQ24070 and enabling our parallel, high current path for the battery to supply the load.
Can you see any possibility that as the chip is disabled, a negative step voltage occurs on the battery and there is a resulting negative going spike (below 0V) at ISET1?
Thanks and Best Regards
Jerry Molnar