This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2595: TPS259541 OVP Didn't Trigger

Part Number: TPS2595

Tool/software:

Hi expert,

Customer set the OV threshold to 14V but still didn't trigger OVP until 15V. 

Would you please have a look and advise what might goes wrong?

 TPS259573_Design_Calculator_RevA_20241101.xlsm

Thanks,

Allan

  • Hi Allan,

    What is the value of EN at the marked region?

    OVLO works based on the comparator at the ENb/OVLO pin in this device. If the voltage level is below the threshold 1.2V typical and 1.27V max, the OVLO won't trigger. This looks like the case here.

    Best Regards,
    Arush