Part Number: LM5023
Tool/software:
The ripple in the circuit above is around 200 mvpp at 5 Ampere, without load 92 mvpp. Load regulation is very good, less than 0.5%.
How do I reduce the ripple to at least 1% or 120 mvpp?
If I increase capacitance, the regulation stops working correctly, and the same is true if I insert inductance.
Thanks