Other Parts Discussed in Thread: LMZ31710, TPS54824
Tool/software:
Hi, expert:
I see TPSM843A22 could support switch internal clock to external sync, I hope to know how about the dynamic performance when switch to external sync or switch to internal clock, do you have some test result could provide?
I know the TPSM843A22 is the better generation than LMZ31710, for LMZ31710 "It is not recommended to switch from CLK mode back to RT mode because the internal switching frequency drops to 100 kHz first before returning to the switching frequency set by the RT resistor (RRT)" I want to ask what have changed in TPSM843A22, why TPSM843A22 could support switch, I need get this information and promote TPSM843A22 to my customer.
In addition, TPSM843A22 only could support five selectable lever switching frequencies: 500 kHz, 750 kHz, 1 MHz, 1.5 MHz, and 2.2 MHz, right? not support any external frequency that supports 500-2.2M, like 600Khz.
Thanks!